Feedback_Limit_Speed

Feedback_Limit_Speed

Address:Address: 10280 (2828H)
Type: Unsigned32
Access: Read/Write
Unit: rpm
Range: Unsigned32
Default Value: 10000
Store Supported: Yes
Description: This value is used for Feedback feature and define the maximum motor speed. If the speed became higher of the limit, the motor current is reduced to limit the speed.
Notes: See Closed Loop Modality for details.